FOR IMMEDIATE RELEASE No. 3183
Will support high-speed transmissions and large-capacity of optical fiber communication
TOKYO, March 7, 2018 – Mitsubishi Electric Corporation (TOKYO: 6503) announced today that it will begin shipping a laser-diode transmitter optical subassembly (TOSA) capable of supporting 400Gbps optical transmissions on April 1. The new TOSA, when used in a set of two, can be used in the industry's first electro-absorption modulated laser diode (EML)-TOSA solution for IEEE 400GBASE-LR8 applications. The device will be displayed at the Optical Fiber Communication Conference and Exhibition 2018 (OFC) in San Diego, California from March 13 to 15.
Compact Integrated 400Gbps EML-TOSA FU-402REA-41 (top) and FU-402REA-42 (bottom)
In response to the demand for increasing data capacity, Mitsubishi Electric's new laser-diode TOSA offers 400Gbps transmission capability for large-capacity communication facilities (data centers, etc.) and high-speed optical transmission networks.
Product | Model | Features | Shipment date |
---|---|---|---|
Compact Integrated 400Gbps EML-TOSA | FU-402REA-41 (for short wavelengths) |
- EML for 1273.54, 1277.89, 1282.26 or 1286.66nm wavelength - LC receptacle |
April 1, 2018 |
FU-402REA-42 (for long wavelengths) |
- EML for 1295.56, 1300.05, 1304.58 or 1309.14nm wavelength - LC receptacle |
Note that the releases are accurate at the time of publication but may be subject to change without notice.