MITSUBISHI ELECTRIC Changements pour le meilleur

Agile, robust, sustainable – the Mitsubishi Electric robot turns 25 in the production of Durable

A success story

For over 50 years, office products manufacturer Durable has been producing display panels – pockets with frames that serve as an information medium.

At the end of the 1990s, the assembly was automated with a MELFA industrial robot from Mitsubishi Electric that celebrates its 25th anniversary next year.

There is still no reason for the senior robot to retire, but when the time comes, the successor generation of the MELFA FR series industrial robots will seamlessly take over.

Challenges in the automation of the manufacturing processes of Durable

Little space for robots

For the full automation, the complete feeding and handling process of the display panels from Durable had to be accommodated within the production cell. So there was little space for the robot.
Ultimately, the Mitsubishi Electric robot was compact and manoeuvrable enough to be able to perform all the necessary movements within the limited space.

Severe mechanical stress on the robots

Another major challenge was the high mechanical stress on the robots during application.
The robot grips and handles parts weighing just a few grams, but its own mass leads to loads on the gearbox and brakes due to short cycle times, high dynamics and large lever forces.
To prevent breakdowns, Durable therefore operates a tight maintenance programme and comprehensive spare parts inventory.

Solution: Mitsubishi Electric articulated robot passes the endurance test

Endurance test passed: the demanding application with constant reversing makes full use of the speed and range of the six-axis kinematics of the articulated arm robot.
In this process, the robust technology from Mitsubishi Electric has proven to be long-lasting and has more than proved itself in continuous operation.
The robot's operating data is used for condition-based maintenance to further ensure its availability.

The robot application is a complete success.

The result: production could hardly be more sustainable

Thanks to automation, Durable is still able to produce its display panels cost-effectively with the Mitsubishi Electric robot.The Durable application is a good example of how a quality-conscious and far-sighted investment policy - in this case, full automation using Mitsubishi Electric robots - can future-proof production equipment and thus also conserve resources.

Get in touch
Sélectionner...
Les champs marqués d'un * sont obligatoires.

... and what happens next? Easy conversion to new robot series possible

Conversion to the FR series of vertical articulated robots from Mitsubishi Electric

No one is thinking of retiring the veteran just yet, but the new FR series of vertical articulated arm robots will follow, so that Durable can benefit from the technical advances of recent decades.

The production manager is relaxed about the day of the changeover. Based on the experience of the users in the Durable production, the change is quite simple except for the programming environment. A cell has already been converted to an industrial robot from the current series.

Highlights of the FR series of MELFA industrial robots from Mitsubishi Electric

Modernisation to the new MELFA FR robot series with internal cable routing, improved technical data and more possibilities for optimisation is easy.

User-friendly teaching boxes ensure ease of use during commissioning, while the modern operating instructions are provided in the form of easy-to-understand videos and online tutorials.

Find out more about the highly dynamic FR series:

Next-generation intelligent features using AIEnhanced security features for safe, collaborative work applicationsSeamless integration into the IT environment
MELFA SmartPlus offers higher accuracy and faster start-up times, which simplifies installation and enables advanced tasks such as temperature compensation, a force-torque sensor, calibration support, etc.Comprehensive safety features, including position and speed monitoring, enable collaboration with humans at work.The MELSEC iQ-R compatible robot control system and the integrated e-F@ctory FA solution offer seamless integration of robots and IT systems.

Do you have any further questions?

Do you have any questions or need advice? We will be very happy to help you.
Please complete the fields marked with *.

Les champs marqués d'un * sont obligatoires.

Our Stories

Robot in Robotronic Factory

2026-02-01

NEWCan robots fill the pharmaceutical supply gap?

Robotronic

Regardez la vidéo sur YouTube
#Life Science#Industrial Robots - MELFA#Servo motors#Human-Machine Interfaces (HMIs) - GOT
Mitsubishi Electric Roboter with Durable Team

2025-01-01

NEWMitsubishi Electric robot at Durable turns 25

Durable

EN
#Manufacturing#Industrial Robots - MELFA
E-Car Cockpit - Noffz case study

2024-06-01

Industrial robots as an unusual measuring tool for testing radar sensors

Noffz GmbH

ENDE
#Automotive#Digitalisation#Industrial Robots - MELFA
Coating example - Singulus

2022-12-01

Robotics‑powered decorative coating from a single source

Singulus Technologies AG

DE
#Packaging#Material Handling#Servo motors#Programmable Controllers MELSEC#Industrial Robots - MELFA
Cutting a cake with a robot

2019-07-06

Robot duo cuts cakes & much more

Western Mechanical Handling (WMH)

DE
#Food & Beverage#Machine Building#AC Servos-MELSERVO#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA#Controllers
Martinshof Poka Yoke

2018-11-01

Poka Yoke: Error-free manual workstations

Werkstatt Bremen - Martinshof

DE
Regardez la vidéo sur YouTube
#Automotive#Material Handling#Controllers#Human-Machine Interfaces (HMIs) - GOT#Industrial Robots - MELFA