MITSUBISHI ELECTRIC Changes for the Better

Are you on the lookout for solutions that boost the availability and utilisation of the critical assets on your aggregates processing plant?

Keeping critical plant assets running and available is fundamental to a plant operating at optimum efficiency and achieving required production levels.

Predictive maintenance is the digital, intelligent approach to maintenance as it uses analytics based on diagnostic data from each asset to predict when assets require maintenance or indeed are about to fail. Armed with this knowledge asset maintenance can be planned around production schedules to optimise both availability and utilisation and avoid unnecessary maintenance shutdowns.

Mitsubishi Electric’s proven, robust automation solutions enable you to realise advanced condition monitoring and predictive maintenance strategies to help you drive the visibility, accessibility and reliability of your critical assets, ensuring that these assets achieve optimum availability and utilisation.

Looking to increase reliability and performance at your plant?

Smart asset monitoring solutions offer a rock-solid approach to optimised maintenance and productivity.

The aggregates industry is characterised by harsh operating conditions and the need to avoid downtime at all costs. Keeping critical plant assets running and available when required is fundamental to a plant operating at optimum efficiency and achieving required production levels.

We are experiencing a fourth industrial revolution which is leading to the creation of what has been dubbed ‘Industry 4.0’ or I4.0.
FAG SmartCheck for End Users and System Integrators.

Cyber Security and Operational Technology (OT)

The move towards digitalisation and reliance on data driven decisions coupled with an increase in cyber related crime means that Cyber Security has become extremely important in our emerging digital world.

Mitsubishi Electric explores how this impacts the OT sector around industrial automation and control systems in terms of the standards and best practises for the key stake holders including asset owners, systems integrators and product suppliers.

Predictive Maintenance: The “low hanging fruit” of the industrial digitalisation process

Predictive and prescriptive maintenance have become key deliverables of the digitalisation process in industrial automation and control.

Advances in Artificial Intelligence (AI) combined with the ability to collect large quantities of data from disparate and remote plant assets means that generation of analytics around predictive maintenance has become much easier to achieve.

Mitsubishi Electric will discuss the growth in capability of predictive maintenance solutions that deliver real value to the asset owner, drawing on their wealth of expertise and automation offerings in this area.

Who knows about the new G5-5 harmonic legislation?

Join us as we look at the new standard, how it differs from G5-4 and how it affects new / existing installations.

Are you aware that G5-5 is a site standard and not a product standard? and as little as 30Kw of none linear load could make your entire site none compliant.

Not only will be covering the standard itself, but what services and products we can offer to make your site compliant.

We Know... Time-Sensitive Networking (TSN)

Industry 4.0 has moved beyond the novelty stage and has become a strategic focus for many companies. While IIoT offers an effective technology platform for Industry 4.0 applications, its foundation is a suitable network with the necessary level of determinism to share all data generated by a process. This transparency depends on convergence, i.e. the ability to combine multiple types of traffic on a single network, which in turn depends on determinism.

The technology that automation is moving towards to address this need for convergence is Time-Sensitive Networking (TSN).

Find out what we know and why we believe TSN should be part of your company's strategy today.

How asset performance helps you

iQ-R PLC

The core for next-generation automation environment.

To succeed in highly competitive markets, it's important to build automation systems that ensure high productivity and consistent product quality.

MELSEC iQ-R is taking a three-point approach to solving these problems: Reducing TCO, increasing Reliability and Reuse of existing assets.

ICONICS

Core to ICONICS’ scalable suite of solutions is its advanced visualization technology to run on any desktop or mobile device, high availability, centralized configuration, and ability to connect to a wide variety of industry standard communication protocols.

Human-Machine Interfaces (HMIs)

The GOT sets global standards in design and technology. A wide variety of lineup meets the needs of production sites.

The GOT boasts advanced functionality, acts as a seamless gateway to other industrial automation devices, all while increasing productivity and efficiency.

Smart Condition Monitoring

With its ready-made Smart Condition Monitoring Kits Mitsubishi Electric offers powerful complete solutions for easy integration into existing applications. 

Compared to conventional monitoring concepts, the modular Plug & Play system does not only analyse classic machine data such as temperature, but also vibration-dependent parameters.

The 800 Series Variable Speed Drives

  • Power sizes 0.1kW to 1.5MW
  • Predictive maintenance functionality
  • Advanced energy saving features
  • Built in multi protocol comms
  • Built in PLC
  • IP55 versions up to 160kW

Inquiries

Select...
We're happy to help!

Please let us know your request. We will get back to you as soon as possible.

Personal Information
The fields marked by a * are mandatory.